This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC12050: Parallel the device

Part Number: UCC12050

Dear Team,

I hope this find you well!

Can I parallel the device?

Any concern here?

BR

Kevin

  • Hi,

    It is ok to use the drawing you show. But the output is between 4.7V and 5.3V. So when parallel two with one 4.7V and one 5.3V, the 4.7V cannot output any power then the total power is less than the twice of each, in the worst case, it is possible just one output power the other does not.