This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for Buck solution with both CC+CV mode control

Dear team,

Did we have Buck solution with CC+CV mode control?

Regulator work under CV mode in normal operation. When trigger to OCP, device will enter in CC mode to keep the output current.

Design condition:

Vin=5~6V

Vout=4.2V

Iout=2A or higher

Regards,

Ben