I need to power a AM3517 from a regulated 3.3V that is coming from off-board. The recommended TPS65023 is way overkill and not made for this configuration. INPUT: regulated 3.3V OUTPUTS: 1.8V @1.0A and 1.2V @1.5A Also need sequencing which includes a switch on the 3.3V because it must come up last. There is also a 2nd 3.3V rail needed for other parts in the system so if not provided, I may add a load switch of some sort for that. Is there a good PMIC part to do this with a minimal footprint?