Part Number: TPS769
Hello,
I have a query on the TPS76950 5V output SOT23-5 Linear regulator. I'm using it at low output current 1 - 2mA and would like to know the approximate typical output voltage tolerance over -20 degree C to +55 degree C. If this is not available I would like to know the typical output voltage setpoint at room temperature.
Kind Regards,
Seamus