Hi,
I designed a flyback converter with the UCC28704. I am using the transformer 750811613. The output of the converter should provide one output of 12V and 1 output of 5V while the auxiliary output should be 20V. Unfortunately, the converter malfunctions. In particular, It swiches-on but and after 3 cycles, the auxiliary voltage jumps by 10V. Afterwards, the controller sends small pulses with very high frequency to the mosfet, until the system is led to overvoltage and swithces-off. In the following link you can find a .psdata file with the results. The output capacitance is 330uF.
Blue: Vdd
Red: Voltage on the source of the Rcs
Green: Voltage on the anode of the auxiliary winding diode
Yellow: Voltage on the anode of the 5V output diode
www.dropbox.com/.../ti1.psdata
Best regards,
Gerasimos