This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5143-Q1: Webench was not cleated on Dual output

Guru 19645 points
Part Number: LM5143-Q1

I confirming to operate LM5143-Q1 on above condition.

⇒Vin: 19V, Dual Vout1: 5V and Vout2: 5V output, Iout1: 8A and Iout2: 8A 

 (I will set fsw:400kHz and Iout(CL): 10A when after Webench operate)

But Wenench was not cleated.

Is above condition not to match LM5143-Q1 specification?

If yes, please let me know about mismatched point. 

Best regards,

Satoshi