This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A52: Design help

Part Number: TPS7A52


TPS7A5201WQRTKRQ1 part is designed as shown in the image above. The enable pin is driven from the open drain enable output of sequencer. The sequencer VCC is 3.3 V. All the enable outputs are pulled high (3.3V)using a 10kohm pull up resistor. I would like to confirm whether my IC will work properly and the discrete components(res, cap) added to each pin will ensure the best performance of my IC