Tool/software: WEBENCH® Design Tools
Hi team,
I wonder how to interpret webench recommended input / output ceramic capacitor value.
When 24V/9V 5.0A simulation is performed, recommended output caps are:
Cap = 47 µF Total Derated Cap = 57 µF VDC = 16 V ESR = 3.04 mΩ Package = 1210 QTY=3
When I try to pick up other capacitor outside of webench for actual design, is it better to use total derated cap value 57uF @ 9V as a reference?
Is this also applicable to input capacitor value?
I'd like to learn how webench nicely picks up input/output cap when the input/output voltage differs from datasheet example.
Regards,
Itoh