Hi,
I am using TPS560430YFQDBVRQ1 in one of my designs with 9V as its input and 5V as output. The total current consumption of the board without any code running is 8 mA. I bypassed TPS560430YFQDBVRQ1 regulator and directly provided 5V to my load through bench power supply and the current consumed by board was 3 mA. It seems like the regulator itself is consuming 5 mA. Is this because the regulator operates in FPWM? Please help me out here.
Thank you!