How can we detect if the attached battery (lead-acid, 2x12=24V, 7.2AH) is disconnected? (Our (medical) equipment is normally running on external power, and the battery is used as an emergency backup. We want to detect if the connection to the battery terminals are lost - in this case the equipment have to warn the user that no backup-battery is available)
Best regards/ Lars Halling