This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3489: LM3489

Part Number: LM3489

Hi everyone.

we have designed using LM3489. Please refer attached images.

in all three cases input is 12 V. for 1st case(1st image) 3.3V output, 2nd case (2nd image) 5V output and for 3rd case (3rd image) 12V is the output

for 12V output, it is working fine. but for 3.3V and 5V output, IC is getting heated when connected to load.

Can anybody please resolve my issue.

1st image

2nd image

3rd image