Hello:
I would like to consult TPS92641. When the analog dimming is zero and the input is 0V at the analog end, the LED has a current of 18mA. When the analog dimming is simulated, the LED cannot be turned off
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello:
I would like to consult TPS92641. When the analog dimming is zero and the input is 0V at the analog end, the LED has a current of 18mA. When the analog dimming is simulated, the LED cannot be turned off
Hi Sir,
Please carefully read the datasheet section 7.3.4 for the true-zero current operation, " For true zero application, an external capacitor is required across the LED string to provide a negative current path for the inductor current loop. "
BR
Sean