Other Parts Discussed in Thread: LM25119
hi sir
Does TPSM831D31 Can output 0.5v~6v /60A?
i need 8 ch dc bus for FPGA
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi sir
Does TPSM831D31 Can output 0.5v~6v /60A?
i need 8 ch dc bus for FPGA
Yes. You can use the 3-phase channel of TPSM831D31 for 0.5V @ 60A. The boot voltage for both channels is 0.5V. You may also program a new boot voltage through PMBus as desired.
hi Sir
the datasheet show • Output Voltage Range: 0.25 V to 1.52 V(may i know max output voltage?)
1• Input Voltage Range: 8 V to 14 V
• Dual Output: 120 A (3-phase) + 40 A (1-phase)
• Output Voltage Range: 0.25 V to 1.52 V
– Programmable in 5-mV Steps
– Differential Remote Sense
– ±0.5% Vref Accuracy with Remote Sense
TPSM831D31 is validated and designed for up to 1.52V output. This limitation is given by the inductor used on the module, to ensure it will not saturate during operation.
I see I have misread your original question. We do NOT recommend TPSM831D31 for up to 6V output.
TI does not have a module which can support this range of output voltages at 60A. Higher current modules will be optimized for low voltage.
Hello, the TPSM831D31 maximum output voltage is 1.52V, so it will not support 6Voutput. For 6Voutput we recommend the LM25119 controller.