This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54JA20: TPS54JA20 unencrypted orcad lib

Part Number: TPS54JA20

Dear Team 

Good day

Our customer need to test the TPS54JA20 with 1.5uH inductor

input, 3.3V, output 1.0v, 8A
The webbench Load transient simulation was failed with 1.5uH inductor

He want to use this regulator for Xilinx FPGA kintex 7 and Ultra
Please provide unencrypted orcad lib or check it is safe to use 1.5uH inductor ?

Best regards

Leon.liu