Hello Experts,
I need to ask a very simple question: I am designing a board with Spartan 3 FPGA (XC3S1000) with some interface ICS from MAX (422 and 232) and a USB micro controller. For FPGA I have designed its power circuit using TPS 75003. In this design the theoretically calculated current requirement for 3.3V (for full design) is about 6 AMP where as the output current of TPS is 3 AMP (current requirement for FPGA is 3 AMP) Please suggest any suitable power management IC for my design (having Spartan 3 FPGA and other interface IC). If I use a separate 3.3 Volt regulator (PTN series) for rest of my design and TPS 75003 for FPGA only I need to add a separate plane for it (one for VCCO and one 3.3V for rest of Interface Chip). Waiting for a quick reply or suggestion.