This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7A4101: Input capacitance value

Genius 17325 points
Part Number: TPS7A4101

Hello,

 

My customer has an question for TPS7A4101.
The datasheet recommends to use 10uF capacitance for input.

In the customer’s system, there is a 100uF capacitance in front of the TPS7A4101 input capacitance(Cin) because they use a half-wave rectifier circuit.
Then they are asking whether they can reduce the input capacitance value from 10uF to 0.1uF.
Is it OK?

 

Regards,

Oba

  • Hi Oba, 

    I would consider the 100uF capacitor to be "remote", and the TPS7A41 does require a "local" input capacitor of 1uF or higher that could affect the stability. I would suggest following the datasheet recommendation and use a 1uF instead of 0.1uF as local input capacitor. 

    Regards, 
    Jason

  • Hello Jason,

    Thanks for your reply.
    What does "remote" mean in this case? Is it distance between 100uF and IN pin of TPS7A41?

    Regards,
    Oba

  • Hi Oba, 

    Yes, you may consider the input capacitor as a decoupling capacitor which needs to as close to the input pin of the LDO as possible. 

    Regards, 
    Jason Song

  • Hello  Jason,

    Even if 100uF is put closely to VIN pin, do you recommend to use 1uF instead of 0.1uF?

    Regards,
    Oba 

  • If the 100uf is put closely to the VIN Pin, you could use 0.1F.

  • Hello Jason,

    Thanks. Let me confirm one thing.

    >I would suggest following the datasheet recommendation and use a 1uF instead of 0.1uF as local input capacitor. 

    You answered 1uF as datasheet recommendation. But the datasheet highly recommend to use 10uF although 1uF can be used.
    Do you thing 1uF is enough in this case because there is 100uF already?

    The TPS7A4101 high voltage linear regulator achieves stability with a minimum output capacitance of 4.7 μF and
    input capacitance of 1 μF; however, TI highly recommends using 10-μF output and input capacitors to maximize
    AC performance.

    Regards,
    Oba

  • Hi Oba, 

    If the 100uF is very close to the input pin, it can be considered as input capacitors, and adding a 0.1uF or 10uF can help further reduce the source impedance at a higher frequency and potentially improve the AC performance as the datasheet stated. But since you already have the 100uF, they become optional. If space and cost allow, it's recommended to have the additional 0.1uF or 1uF. 

    Regards, 
    Jason