Part Number: BQ25606
Other Parts Discussed in Thread: BQ25616,
Hello
I would like to know what happen to RBFET when boost mode is disabled (no OTG).
I would like to use the bq25606 (or bq25616) with a 4.2V(charging voltage) battery.
It is powered from a buck converter (from 24V to 4.5V), so when power supply is disconnected the input of the BQ25606 is still conntected to the buck circuit.
I would like to know what happens to RBFET if i disable the boost operation. Is the BQ25606's input disconnected and RBFET is blocking? If yes, how much is RBFET leaking from output to input in that state?
Thanks
Massimo