Other Parts Discussed in Thread: BQ51003
Hello. Referring to the schematic on EVM-764 Figure 4.1.
We have successfully replicated the core circuit shown there and everything seems to be working OK on a prototype.
We stripped out all the dev features not relevant to us.
Our charging requirement is very light, about 100mA max.
Now we need to do an extreme size shrink on the design and the many parts are not all fitting well.
Here is the main question:
What is the reason for the 3 parallel caps C1, C2, C3 ? Net value is 0.18uF.
Can't we use a single cap 0.2uF?
All of the many caps in that section are 50V, is that really necessary, I am referring to more than C1-C3, there are 11 caps in that area.
C5 is tweaking C4 but is close to tolerance of C4, what will I lose if I delete C5 considering that power is low and efficiency not a priority.
I need any tips to make this as small as possible and reduce component count please.
I can send my schematic but I don't want to post it here
Thanks !