This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: Start of Re-sequence after a shutdown due to a GPI Fault Enable

Part Number: UCD9090A

I've set up a GPI to have the special behavior of GPI Fault Enable and Fault Shutdown rails.

I also checked the Option to enable re-sequencing for that GPI, and to shutdown immediately as the Fault Response.

None of the rails are set up with dependencies, other than Vin on/off.

All my rails are set-up with an On/Off Config of Auto Enable.

When the GPI is de-asserted, the rails shutdown, but never restart.

Does the GPI need to re-asserted before the re-sequence of rails can start?

What other conditions might result in the re-sequence not starting?