hello,
I have a question about Charging Status Indicator (STAT).
When the CHARGING STATE is as follows, the STAT INDICATOR is blinking at 1 Hz.
How is STAT INDICATOR output when Input fault (VBAT = 3.7V <VBUS = 3.79V <VVBUSMIN (typical 3.8V))?
Excerpt from Table 8. STAT Pin State
CHARGING STATE when blinking at 1 Hz is output
Charge suspend (Input overvoltage, TS fault, timer fault, input or system overvoltage)
Boost Mode suspend (due to TS Fault)
best regards