Other Parts Discussed in Thread: TPS92515
Hi,
I am using TPS92515HVQDGQRQ1 in my design. These are the required parameters.
Vin = 12V
Vout = 9.3V (3LEDs in series each of 3.1 forward voltage)
Iout= 1A
I have implemented the circuit using TPS92515HVQDGQRQ1 but not able to achieve desired output. One thing I noticed is the Output average voltage (measured across output capacitor) is 5V and the switching frequency I could measure is 21Hz.
I have attached the snapshot of the design. It will be helpful if I get any suggestion on how to increase the switching frequency.
For now I have tied the PWM1 to VCC and Isolated the load by disabling the load switch (TPS22810TDBVRQ1).
Regards,
Muhammed Shajih