Other Parts Discussed in Thread: TPS40428
Hi Sir,
may we learn from you this issue,thanks.
I use TPS40425+CSD95372AQ5M for application design
Read current and power consumption through GUI, such as 1.8V(operating Two-phase).
The total current is CH#1 plus CH#2, right?
Total power consumption: 1.8*(10.5+9.1) =35.28W
But the GUI shows that CH#1 is 1.814v*10.563A = 19.16W and CH#2 is 1.814v*9.125A≠19.16W (total 19.16+19.16=38.32W).
The results are not consistent. How do we look at this?
How to readout if I use I2C? According to PMBus, is 0x96 Pout?
CH#1 or CH#2 or CH#1 +CH#2 ?