dear
LM5176 provide current 6.5A while input voltage is 13v and 25A while input voltage is 24v,but 5 minutes of aging, the output voltage will fall down to about 8V
Attachment is about LM5176 SCH any advice? thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear
LM5176 provide current 6.5A while input voltage is 13v and 25A while input voltage is 24v,but 5 minutes of aging, the output voltage will fall down to about 8V
Attachment is about LM5176 SCH any advice? thanks in advance
dear
1. At present, we are producing 450W 24V output power. May I ask what is the maximum power of this chip?
2. At present, we use two sets of LM5176 for 225W and 450W 24V in parallel. As a result, two SETS of LM5176 are burned as soon as the power is switched on. The parallel mode is Vin+ and VIN-parallel, and the two sets of Vout+ and Vout-parallel
3. When the power supply has overload protection and short circuit protection, is there any way to realize that when the overload protection or short circuit protection is removed, the output voltage can be restored only after the disconnected power is restarted. At present, the output voltage can be restored automatically after the chip is removed
any advise? thanks in advance
Hello CS kk,
1. I would say that with an output power of 450W you are coming close to the internal driver capability with the external MOSFET gate charges, but this depends on the used MOSFETs.
2. If you are putting 2 different converters with separate voltage loops in parallel, one of them will most probable take all the power and the other one will not do anything. The reason is that they do not have exactly the same output voltage and the one that has a slightly lower reference voltage or slightly different result in the resistor divider will always think that the output is high enough, so it does not need to do anything. You need to define a main and secondary device and connect them according this app note:
3. If I understand your comment correctly, then the MODE pin setting into hiccup mode (R = 93.1 kohm) would solve this issue. In hiccup mode, the converter tries to restart after some time when it got into overcurrent.