In section 7.3.1 of the datasheet, there is a reference to Vo(reg) but I couldn't find any other refernce to the value and tolerance of Vo(reg). Can you help clarify?
Best regards,
Matt
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In section 7.3.1 of the datasheet, there is a reference to Vo(reg) but I couldn't find any other refernce to the value and tolerance of Vo(reg). Can you help clarify?
Best regards,
Matt
Hi Matthew,
This value is not specified with a target value and tolerance. I cannot find any information on this value unfortunately.
In section 7.4.1, it says:
"The device continuously monitors the input voltage, the input current, and the battery voltage. As long as the input voltage is less than VOVP, the output voltage tracks the input voltage (less the drop caused by RDSON of Q1). During fault conditions, the internal FET is turned off and the output is isolated from the input source."
Best regards,
Matt