Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC2818A: How does the PFC compare to the PFC in the UCC28513?

Part Number: UCC2818A
Other Parts Discussed in Thread: UCC28513,

I am designing a PFC for a 400Hz application. A colleague of mine successfully designed a good PFC that drove a Flyback using the UCC28513. I am weighing my options between the 28513 and 2818A. My question pertains only to the PFC portion of the 28513. As far as I can tell the biggest difference is that the 2818A has a soft-start feature for the PFC, which is something I do like. But I am curious how the two compare in terms of THD performance and power factor for a given application.