I am wondering if it is possible to use TL4242 as a constant current sink but without actually using LEDs. I believe I would do this by simply connecting Q directly to REF. It seems like this should work, and the TL4242 would drop all of the voltage from VIN to REF. One concern is that the datasheet mentions protection from short circuit, although gives no further details. What I would be doing is essentially shorting out the LEDs. What is the short circuit protection? Does it simply make sure the part will not overheat? Or does it reduce or disable the output?