Hi TI Team,
I'm currently using 4 LED with 20% segment for SOC indication. I set LEDCHG, but not BLINKMIDPT. And I found that during charging, for example at SOC = 80% ~ 99%, LED4 is blinking not solid until 100%, which seems not exactly match the description in sec 8.1.6 of TRM. Is this as expected or I missed something for the LED setting?
Also, I found that after I stop the charging before FC (e.g. just stop charging at SOC = ~96%), LEDs remain on for roughly 60s which is quite long. Is that possible to decrease this period to e.g. 1s?
Thanks,
Zhihan