This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3870-Q1: Latch mode(CT=0V) operation

Part Number: TPS3870-Q1

Hi expert,

My customer plan to use TPS3870J4080DSERQ1 (0.8V) with latch mode(CT=0V).

They plan to input pulse to CT pin for unlatch.

If they will input over 1.15V voltage continually to CT pin, how does the Reset output work at this timing? (at Sense pin > 0.8V)

In case of the following waveform (datasheet Figure27)

Why will the reset pin be High-Z after unlatch?

I think, The reset output will be low after unlatch, because Sense pin=1.2V (= OV condition).

Thanks

Muk

  • Hi Muk,

    Yes, if the CT pin receives a voltage that is above 1.15V, the RESET signal will be de-asserted (high state) but it depends on the voltage of SENSE pin.  If the SENSE voltage is above 800mV * (+ 0.25% - typ) or (worst case VIT+(OV) =  837.6mV (4.7%)), /RESET will stat asserted even after you apply a voltage greater than 1.15V on the CT pin.

    In figure 27, /RESET is at high-z because the sense voltage is not above VIT+(OV) and the application is monitoring a rail voltage of 1.2V.

    Ben

  • Thank you Ben-san,

    Is it meaning, in Figure27, the SENSE waveform(green, ch3) is monitoring the voltage rail of 1.2V? (it is  not SENSE pin voltage)

    Because, TPS3870 line up are 0.8Vmon and 3.3Vmon only.

    This is a very confusing waveform name...

    Thanks

    Muk

  • Hi Muk,

    I would like to take this conversation offline.  Please close the thread and I will reach out to you via internal email.  Thank you.

    Ben

  • Ben-san

    Thank you for your answer.

    Muk