Dears
Schematic diagram of charging management, where R6 connected to PRETERM has tried 0Ω and 1KΩ, but the pre-charge current is very low;
According to the existing configuration, the fast current should be 300mA;
When the lithium battery (3V~4.2V) enters over-discharge, the pre-charge current is too small, and it takes a long time to pull the lithium battery from 0V back to the effective voltage output.
Please help to find out the reason and how to modify it?
It's urgent case. Please help support today.
Thanks.