This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Vadym,
VEDV corresponds to a threshold on the BAT pin. The BAT senses a divided down voltage of the battery, dependent on the resistor divider used to program the charge regulation voltage. MCV is a similar threshold which is defined as VMCV = 0.8 ∗ VCC ± 30mV. BAT does not sense the true battery voltage, as this is a charge controller.
Hi Kedar,
Yes, I see that V_CELL is not an actual battery voltage but V_BAT voltage that's defined by voltage divider between BAT and SNS pins on the BQ2004.
So for 12-cell RB1 = 40k, which at nominal battery voltage(14.4V) an actual V_CELL = 12V.
The DCMD input is used to command discharge-before charge via the DIS output. Once activated, DIS becomes active (high) until VCELL falls below VEDV, at
which time DIS goes low and a new fast charge cycle begins.
The problem I'm running into is that I need to have ability to terminate discharge at any desired battery voltage threshold(V_PACK). But it seems that discharge voltage is fixed by V_EDV, where V_EDV = 0.4*V_CC = 0.4*5= 2V.
So that means that V_CELL needs to drop below 2V for discharge to be terminated. Which means that at V_CELL= 2V, an actual battery pack voltage will be V_PACK=2.4V! This is disastrous low discharge voltage for 12-cell NiMH battery. Is there a way to control depth of discharge with BQ2004?
I greatly appreciate your help, Vadym.
Hi Vadym,
This is an older part, and unfortunately has an inbuilt discharge threshold. There is no configurability here