Hi all,
I am using a MSP430 with 2 AAA battries. MSP is in deep sleep mode for approx. 1 sec then wakes-up upon hal sensor interrupt, then MSP trigger a coil using BSS138N MOSFET. While sleeping MSP consumes 1uA and .5mA when woked up. Current cosumption when coil is triggered: 3mA for 200ms
Now, I realize that I need more volts for this coil than 3 volts. MOSFET is connected to external power supply of 9V to 12 Volts and works great.
I am looking for a DC/DC converter suggestions. Below is my wish list:
Extremely low BOM, preferably includes some sort of switch so I don't have to use BSS138N, extremly low current consumption when sleeping, module for factor also acceptable as long as it is not BGA.
Thank you very much,
Jay