I study my inrush current problem (with help from Shreyas Dmello) and I think i can solve it with the TPS1HHB08A-Q1 (high inrush current >15A and only 8A available). I want to use the TPS1HB08A-Q1 between the TI boost convertor (WEBENCH using LM3478) an the TI H-Bridge (DRV8873H) for powering an Peltier Element (TEC1-12706). I have no control line available so i have to adjust it static. I have connected it as follows (see attachment).
But something else why are all the parts (TPS1HB08A-Q1) in days gone in all warehouses (Mouser and TI store)!!! I need a few to test, because production will start in a few weeks.
Best Regards,