This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24295: Low VSYS

Part Number: BQ24295


Hi Team, hoping for your comment about this situation. 

After charging or manually turning off BATFET, the VSYS current is limited heavily (~200mA) and not providing enough power (~1A) to the system. If we reset the system by toggling the system power switch, the current limit disappears for a moment but starts limiting the current soon after. As soon as we remove VBUS, the battery takes over and provides enough current.

We have set the input current limit to 3A. VBUS input voltage is stable even while charging at 2A, so that is not the problem either.

Thank you in advance.

-Mark