This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110EVM-796: Usage of automated GPC Cycle with BQ studio?

Part Number: BQ34110EVM-796
Other Parts Discussed in Thread: BQ34110, EV2400, BQSTUDIO

I saw that BQ studio supports an automated GPC Cycle.In my current setup, I use EV2400 and bq34110 EVM with an external charger and load that are connected to the Relay module. When I start the GPC Cycle I only get one impulse(for approx. 1s) at the beginning of each step (charging or discharging).

Is this expected behavior for the automated mode?

I would need high logic level present for as long as charging or discharging is needed.

https://www.ti.com/lit/ug/sluu446d/sluu446d.pdf?ts=1605478288581&ref_url=https%253A%252F%252Fwww.ti.com%252Ftool%252FEV2400