I want to see the inductor current waveform of the LM5170EVM-BIDIR board. The Userguide suggest to put "Current probe capable of 50 A is required to monitor the inductor current via a wire loop inserted to the non-switching side of the inductor".
1. Is there any ports/points available where we can make/insert the wireloop.
if not,
Please suggest where should we put the current probe.
Regards,
Siddheswar Sen