This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28220: Soft Start

Part Number: UCC28220
Other Parts Discussed in Thread: UCC28221

Hi,

Our customer is using UCC28220. He finds that there is no Soft-Start function. He applies the power on VDD first and then increasing VIN voltage to 240V. Could you please tell us how to get the Soft-Start function? And the normal power up sequence?

Thanks.

Kevin Xiong

  • Hi Kevin! 

    Thanks for reaching out and for your interest in the UCC28220. Do you have a capacitor connected to the SS pin? The sizing of this capacitor (as well as the sizing of the CHG resistor) determines the soft start speed. 

    The VIN pin is a NC pin on the UCC28220, is your customer maybe using the UCC28221? 

    Thanks again for getting in touch, I look forward to talking more soon!  

    Aidan Davidson