Hi,
I'm using the QuickStart Calculator.
Is the phase margin about 22° or 202° when the bode plot is the following?
Best Regards,
Kuramochi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm using the QuickStart Calculator.
Is the phase margin about 22° or 202° when the bode plot is the following?
Best Regards,
Kuramochi
Hi Kuramochi,
Thanks for reaching out with your question and for considering the LM%155 in your design.
The plot is showing the phase margin relative to 0 deg. In the screenshot above the phase margin is only 22 deg. I suggest increase the value of CCOMP. This is lower the frequency of the compensation zero (fz_ea) and increase the phase margin.
Please let me know if you have any questions.
Thanks,
Garrett