This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS563210A: Soft start time accuracy

Part Number: TPS563210A

Hi team,

I have a question about the soft start time.

My customer connected 0.047uF to SS-pin and expected 5.2ms soft start time(10% to 90% of Vout). However, the measured soft start time was 6.64ms. The variation of the 0.047uF capacitor is +22%(max), but they tested room temp condition, so the capacitance shouldn't change much. Therefore, customer thinks that there are other factor for the longer soft start time. I believe that Iss variation affected this soft start time. Is my understanding correct?

Regards,

Yamaguchi