Hi there,
Two quick questions:
1. Can this device handle a single 50Ah 3.7V battery (I assume using the X10 mode?)
2. Can it handle a battery which is connected to a protection circuit (PCM) or will it work well only connected to the actual cell itself?
Thank you,
Nir.