Team,
Can you please clarify Vcc specs:
Bit of ambiguity in the datasheet in regards to Vcc for this part. There doesn't seem to be an operating range for Vcc listed specifically anywhere in the datasheet, just absolute max.
It states that the internal LDO output for Vcc is 5.2V and if you want to provide your own for power savings then it "must be within the 4.75-V to 5.5-V regulation range"
But all I/O thresholds are under the test condition "VCC = 2.7V to 5.5V". I also don't see any verbiage that prevents input and output from being less than 5V?
I stumbled across this when trying to verify if our 3v3 i2c pullups already in place would be acceptable.
Basically, we just need to know:
- if 3v3 i2c pullup is acceptable when using internal 5V LDO?
- also if it would be possible to power Vcc from our 3v3 rail (ambiguous)?
Thanks
Viktorija