This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMQ61460-Q1: Current limit

Part Number: LMQ61460-Q1

Hello team,

I have a question about LMQ61460-Q1.

My customer wanted to use BUCK as the below condition.

Does this device support 6A at any condition such as duty cycle, temperature?

They wanted to confirm perfectly about load current because their production may be left short time.

4. Conditions :

1)

- Vin = 8~24V.  (typ 13.5v)

- Top = -40~ 105 ℃

2) Load 조건

- Vout = 7V

- iout = Max 5A 

Thank you.

Best Regards,

Kevin Shin