This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610-R1: Inquiries about Battery Learning.

Part Number: BQ28Z610-R1

1. BAT  Configuration.

    1)  PACK  :  2S-1P

    2)  F/G  :  BQ28Z610-R1

2. BAT Spec : INR21700-50E
   1)  Standard discharge Capacity : 4900mAh
   2)  Charging Voltage : 4.2V
   3)  Nominal Voltage : 3.63V
   4)  CHEM ID : 2591

3. BAT CEL Protection
   1)  OCD  :  5.1 A (Recovery 0 mA)
   2)  OCC  :  4.0 A (Recovery 100 mA)
   3)  COV  :  4.2 V (Recovery 4.05 V)
   4)  CUV  :  3.0 V (Recovery 3.15 V)

4. BAT PACK Voltage Range
   1)  Max charge voltage : 8320mV  (4.16V per cell)
   2)  Max discharge voltage : 6600mV (3300mV per cell)

5. Quetion   (Inquiries about Battery Learning)

  (1)  Do I only need to learn BAT once?   Or do I have to do it several times?

        ㅡ  The more I learn BAT, the more sophisticated it gets?

  (2)  Do I have to learn BAT in cold conditions?

  (3)  Before creating a golden image, what parameters must be changed?

        ㅡ  I want to change the Protection/Life time/Charging voltage/Discharging voltage.

        ㅡ  I know "I need to change the update status to 02".   Correct?

  (4)  After creating the golden image, can I change several parameters?  ​​(Full Charge/Discharge Voltage/Protection Value, etc.)

        ㅡ  If I change the Protection/Gauge setting, do I need to repeat 'Battery-Learning' from the Beginning?

        ㅡ  Or, can I just modify the registers in the golden image?

             (Learning/Protection : 3V-4.2V  //  Actual use: 3.3V-4.16V)  (Per Cell)

  (5)  If I create GOLDEN IMAGE, is there no need to enter the 'CHEM ID' in mass production afterwards?

 

  (6)  Do I have to upload 'Golden-image' files on TI website?

        Or can I use the 'Golden-image', right away?

        When I get a reply from TI, can I overwrite the file and use it?

  (7)  If Cell-Balancing is not performed at '0x06' when the [Update-State] is 2-CELL,

        should we learn additional charge/discharge cycles to move to '0x0E'?

        ㅡ  is this absolutely necessary?

  (8)  I put the Chem ID of my cell and started the cycle. Should I use the "Gauging Parameter Calculator"?

        ㅡ  Should I use BQ Studio's GPC Packer?

  (9)  Upload our 'Golden-image'. Please check.

2610_1_01-bq28z610R1.zip