This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24773: Some problems with settings

Part Number: BQ24773

Hi 

Questions 1~3, please help confirm
1). Can IADP/IBAT/PMON use 1.8V ADC?
2). Can PROCHOT be controlled by 1.8V?
3). How is ILIM calculated? and VILIM divider

  • Hi Gareth,

    1) The IADP, IBAT, and PMON output voltages are clamped below 3.3 V, so it is best if the ADC can read voltages up to 3.3 V. This way, the ADC can read the full range of possible IADP/IBAT/PMON voltages instead of maxing out at 1.8 V.

    2) Yes, it is fine to use a 1.8 V pull-up rail for /PROCHOT.

    3) Please take a look at the ILIM pin description below, which provides the formula. V(ILIM) is set by the resistor divider values.

    Best regards,

    Angelo