Hi Team,
Could you tell me the "unit" of Tss ?
The right side unit of Eq(2) is (mF * V / A), so I understand that the left side unit will be (ms), is that correct?
But when I calculate it as an example, for Css=3.3nF, Vf = 0.6, Iss= 5uA, this is a bit confusing because (3.3*0.6)/5 = 0.396(ms) < 1.3ms(default).
Regards,
Takashi Oanwa