Hi,
I am trying to determine the coefficients to use with a non 103AT thermistor.
I have found the Excel tool in slua398, but I'm having difficulty getting it to work even if I put in the default 103AT parameters.
One confusing thing is that the thermistor on the bq34110 pulls the TS pin up to the 2.5V reference. The technical reference manual then describes a pull down being implemented internally and the data sheet says that that TS pin input impedance is 5k when the pull down is on.
The sketch given in Thermistor Coefficient Calculator.xls from slua398 shows the TS pin with a fixed pull up and the thermistor pulls this to ground.
How do I set the parameters in the calculator to account for this difference? If I put the 103AT resistance curve in I would expect the parameters generated to match the default ones, but I can't get them anywhere near at the moment.
Thanks,
Simon