Hi,Ti team:
we use TLC5973 to driver RGB LED,we design a FPC which length about 700mm.We total use 8 pcs TLC5973 in the FPC.all of them driver 4 series and 8 parallel LED,The driver circuit is 20mA and the VLED is set 14.4V,The schematic is show below.
When we test RE for the product,the data is beyond the standard much,and the frequency is 12MHZ frequency doubling which is TLC5973 Internal GS oscillator frequency. We try many method but can not solve the questio.When we remove the 5973 and drive by VLED directly.The question is disappear.So we think the re question was cause by the 5973.
Have you ever seen anything like this before,Are there any improvement measures and Suggestions?
As the project is urgent, we hope to get your reply as soon as possible
The relevant test data and schematic diagram are attached below