Good morning,
I am writing to you because I am looking for an SMD chip through which to adjust the temperature of the heaters(resistor foils). For example, my idea was an SMD voltage regulator, but if there is something more suitable even better. The voltage regulator should:
- support an input voltage in the range (approximately) 5-12V and an output voltage that may vary from maximum voltage to drop down to approximately its 50%.
- be “programmable real-time”, i.e. having the ability to adjust its output based on commands via I2C or SPI from a microcontroller.
-
Do you think there might be something like this in your catalogs?
Many thanks in advance,
Best regards,
Gianluca Milani