Hello Guys,
Good day.
Our customer is using LM117H in their design. They are dissipating across the device 10V*20mA~0.2W. They are operating in a vacuum chamber (2*10^-6 mbar) at 25degC.
They mounted a thermocouple on the metal can (top flat surface) region and this thermocouple measured the temperature (in above vacuum condition) to be 70degC. To calculate junction temperature, should they consider the above temperature with theta-ja (186degC/W) or theta j-c (21degC/W)?
In addition to this, is there any limit on the power dissipation of the PFM version? The datasheet says 2W, "but limited internally". What is this internal limit - at what power/ current/temperature?
Thanks in advance!
Art