Hello,
I am sorry to disturb you. I have used the ucc21750 to design a driver board and it works well for a long time. However, it doesn’t output the square signal yesterday when I turn on the 5V power supply, and I smelled something. My power stage is a T-Type inverter so I need twelve ucc21750 for my topology. Unfortunately, four of them were troubled and the phenomena were the same. The output of the controller is 4V pwm signal but after a RC the input of the ucc21756 is 1.3V pwm signal as shown in the figure. I think the ucc21750 is troubled but the reason is confusing.