This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ28Z610: Bq28z610: RM,FCC,RSOC is Not Stable. The value changes approximately each time

Part Number: BQ28Z610
Other Parts Discussed in Thread: TEST2, , GPCCHEM

Hi

I am using bq28z610 with Panasonic NCR 18650f(2900 mah) Battery. I have completed the learning cycle and the full charge capacity value is good and the SOH is 94%. So everything is OK. But when I connected with real-time production, the problem arose.

My product average current value is 10-12 ma/h, and when data is sent or received with a 4G modem, only that time the current value will be above 200mah(Spike Load). Simultaneous charging (solar panel) and discharge process are worked.

problem1:When the morning sunlight comes up, so the charging process begins. That time suddenly changes the value of RM, FCC and RSOC. This condition occurs every day, so the value (RM, FCC and RSOC) increases or decreases day by day.

problem2:There is no charge at night, so the discharge process only works at that time. But the remaining capacity value is not changed. The value did not change for several hours. This condition is not possible because the average current is 12ma / h . The value changes after five or six hours.

Why does this value(RM, FCC and RSOC) change? This is a big issue for my product.

My testing Process:

Test1: I only use the charging process, no change in value (FCC), then I use the discharge process, no change in value (FCC). No big difference, so everything is fine. The problem occurred when I tested it in real-time (simultaneous charging (solar panel) and discharge process). There is a big difference in FCC value from day by day.

Test2: Real-time Test(Simultaneous charging (solar panel) and discharge process). I tried to enable a smooth function and disabled the smooth function, but there were no changes. The same problems occur.

My Doubt: A smooth function that is enabled will calculate(Flt RemCap) the True RemCap value and then display the RM, is this correct?

A smooth function disabled, the True RemCap value Displays the RM directly, is this correct?

Below is the bq28z610 configuration file and the learning cycle log file attached.

* Texas Instruments Data Flash File
* File created Wed Nov 04 08:45:26 2020
*
* Device Number 2610
* Firmware Version 0.17
* Build Number 22
* Order Number 0
*
* bqz Device Number 2610
* bqz Firmware Version 0.17
* bqz Build Number 22
*
* Field Order: Class name, Subclass name, Parameter name, Parameter Value, Display Units
"Calibration","Voltage","Cell Gain","12126","-"
"Calibration","Voltage","Pack Gain","51754","-"
"Calibration","Voltage","BAT Gain","49155","-"
"Calibration","Current","CC Gain","10.004","mOhm"
"Calibration","Current","Capacity Gain","10.003","mOhm"
"Calibration","Current Offset","CC Offset","64","-"
"Calibration","Current Offset","Coulomb Counter Offset Samples","64","-"
"Calibration","Current Offset","Board Offset","0","-"
"Calibration","Current Offset","CC Auto Config","07","hex"
"Calibration","Current Offset","CC Auto Offset","0","-"
"Calibration","Temperature","Internal Temp Offset","0","°C"
"Calibration","Temperature","External1 Temp Offset","0","°C"
"Calibration","Internal Temp Model","Int Gain","-12143","-"
"Calibration","Internal Temp Model","Int base offset","6232","-"
"Calibration","Internal Temp Model","Int Minimum AD","0","-"
"Calibration","Internal Temp Model","Int Maximum Temp","6232","0.1degK"
"Calibration","Cell Temperature Model","Coeff a1","-11130","-"
"Calibration","Cell Temperature Model","Coeff a2","19142","-"
"Calibration","Cell Temperature Model","Coeff a3","-19262","-"
"Calibration","Cell Temperature Model","Coeff a4","28203","-"
"Calibration","Cell Temperature Model","Coeff a5","892","-"
"Calibration","Cell Temperature Model","Coeff b1","328","-"
"Calibration","Cell Temperature Model","Coeff b2","-605","-"
"Calibration","Cell Temperature Model","Coeff b3","-2443","-"
"Calibration","Cell Temperature Model","Coeff b4","4696","-"
"Calibration","Cell Temperature Model","Rc0","11703","-"
"Calibration","Cell Temperature Model","Adc0","11703","-"
"Calibration","Cell Temperature Model","Rpad","0","-"
"Calibration","Cell Temperature Model","Rint","0","-"
"Calibration","Current Deadband","Deadband","3","mA"
"Calibration","Current Deadband","Coulomb Counter Deadband","9","116nV"
"Settings","Protection","Protection Configuration","00","hex"
"Settings","Protection","Enabled Protections A","57","hex"
"Settings","Protection","Enabled Protections B","35","hex"
"Settings","Protection","Enabled Protections C","14","hex"
"Settings","Protection","Enabled Protections D","0c","hex"
"Settings","Permanent Failure","Enabled PF A","00","hex"
"Settings","Permanent Failure","Enabled PF C","00","hex"
"Settings","Configuration","Charging Configuration","01","hex"
"Settings","Configuration","Temperature Enable","03","hex"
"Settings","Configuration","DA Configuration","11","hex"
"Settings","Configuration","FET Options","20","hex"
"Settings","Configuration","I2C Gauging Configuration","07","hex"
"Settings","Configuration","I2C Configuration","00","hex"
"Settings","Configuration","Power Config","00","hex"
"Settings","Configuration","IO Config","02","hex"
"Settings","Configuration","SOC Flag Config A","0cff","hex"
"Settings","Configuration","SOC Flag Config B","ff","hex"
"Settings","Configuration","Balancing Configuration","1d","hex"
"Settings","Configuration","IT Gauging Configuration","26df","hex"
"Settings","AFE","AFE Protection Control","70","hex"
"Settings","AFE","ZVCHG Exit Threshold","2200","mV"
"Settings","BTP","Init Discharge Set","150","mAh"
"Settings","BTP","Init Charge Set","175","mAh"
"Settings","Charger","Device Address","d4","hex"
"Settings","Charger","Voltage Register","0c","hex"
"Settings","Charger","Current Register","0a","hex"
"Settings","Charger","Broadcast Pacing","15","s"
"Settings","Manufacturing","Mfg Status init","0018","hex"
"Protections","CUV","Threshold","2500","mV"
"Protections","CUV","Delay","2","s"
"Protections","CUV","Recovery","3000","mV"
"Protections","COV","Threshold Low Temp","4500","mV"
"Protections","COV","Threshold Standard Temp","4500","mV"
"Protections","COV","Threshold High Temp","4500","mV"
"Protections","COV","Threshold Rec Temp","4500","mV"
"Protections","COV","Delay","2","s"
"Protections","COV","Recovery Low Temp","4300","mV"
"Protections","COV","Recovery Standard Temp","4300","mV"
"Protections","COV","Recovery High Temp","4300","mV"
"Protections","COV","Recovery Rec Temp","4300","mV"
"Protections","OCC","Threshold","2000","mA"
"Protections","OCC","Delay","6","s"
"Protections","OCC","Recovery Threshold","-200","mA"
"Protections","OCC","Recovery Delay","5","s"
"Protections","OCD","Threshold","-3500","mA"
"Protections","OCD","Delay","6","s"
"Protections","OCD","Recovery Threshold","0","mA"
"Protections","OCD","Recovery Delay","5","s"
"Protections","AOLD","Recovery","5","s"
"Protections","AOLD","Threshold","ff","hex"
"Protections","ASCC","Recovery","5","s"
"Protections","ASCC","Threshold","77","hex"
"Protections","ASCD","Recovery","5","s"
"Protections","ASCD","Threshold 1","77","hex"
"Protections","ASCD","Threshold 2","f7","hex"
"Protections","OTC","Threshold","85.0","1°C"
"Protections","OTC","Delay","2","s"
"Protections","OTC","Recovery","60.0","1°C"
"Protections","OTD","Threshold","85.0","1°C"
"Protections","OTD","Delay","2","s"
"Protections","OTD","Recovery","60.0","1°C"
"Protections","UTC","Threshold","-25.0","1°C"
"Protections","UTC","Delay","2","s"
"Protections","UTC","Recovery","-15.0","1°C"
"Protections","UTD","Threshold","-25.0","1°C"
"Protections","UTD","Delay","2","s"
"Protections","UTD","Recovery","-15.0","1°C"
"Protections","PTO","Charge Threshold","2000","mA"
"Protections","PTO","Suspend Threshold","1800","mA"
"Protections","PTO","Delay","1800","s"
"Protections","PTO","Reset","2","mAh"
"Protections","CTO","Charge Threshold","2500","mA"
"Protections","CTO","Suspend Threshold","2000","mA"
"Protections","CTO","Delay","54000","s"
"Protections","CTO","Reset","2","mAh"
"Permanent Fail","SOV","Threshold","4500","mV"
"Permanent Fail","SOV","Delay","5","s"
"Permanent Fail","CFET","OFF Threshold","5","mA"
"Permanent Fail","CFET","OFF Delay","5","s"
"Permanent Fail","DFET","OFF Threshold","-5","mA"
"Permanent Fail","DFET","OFF Delay","5","s"
"Advanced Charge Algorithm","Temperature Ranges","T1 Temp","-20","°C"
"Advanced Charge Algorithm","Temperature Ranges","T2 Temp","5","°C"
"Advanced Charge Algorithm","Temperature Ranges","T5 Temp","10","°C"
"Advanced Charge Algorithm","Temperature Ranges","T6 Temp","20","°C"
"Advanced Charge Algorithm","Temperature Ranges","T3 Temp","35","°C"
"Advanced Charge Algorithm","Temperature Ranges","T4 Temp","55","°C"
"Advanced Charge Algorithm","Temperature Ranges","Hysteresis Temp","1","°C"
"Advanced Charge Algorithm","Low Temp Charging","Voltage","4000","mV"
"Advanced Charge Algorithm","Low Temp Charging","Current Low","132","mA"
"Advanced Charge Algorithm","Low Temp Charging","Current Med","352","mA"
"Advanced Charge Algorithm","Low Temp Charging","Current High","264","mA"
"Advanced Charge Algorithm","Standard Temp Charging","Voltage","4200","mV"
"Advanced Charge Algorithm","Standard Temp Charging","Current Low","1980","mA"
"Advanced Charge Algorithm","Standard Temp Charging","Current Med","4004","mA"
"Advanced Charge Algorithm","Standard Temp Charging","Current High","2992","mA"
"Advanced Charge Algorithm","High Temp Charging","Voltage","4000","mV"
"Advanced Charge Algorithm","High Temp Charging","Current Low","1012","mA"
"Advanced Charge Algorithm","High Temp Charging","Current Med","1980","mA"
"Advanced Charge Algorithm","High Temp Charging","Current High","1496","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Voltage","4100","mV"
"Advanced Charge Algorithm","Rec Temp Charging","Current Low","2508","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Current Med","4488","mA"
"Advanced Charge Algorithm","Rec Temp Charging","Current High","3520","mA"
"Advanced Charge Algorithm","Pre-Charging","Current","100","mA"
"Advanced Charge Algorithm","Maintenance Charging","Current","50","mA"
"Advanced Charge Algorithm","Voltage Range","Precharge Start Voltage","2500","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Low","2900","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Med","3600","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage High","4000","mV"
"Advanced Charge Algorithm","Voltage Range","Charging Voltage Hysteresis","0","mV"
"Advanced Charge Algorithm","Termination Config","Charge Term Taper Current","250","mA"
"Advanced Charge Algorithm","Termination Config","Charge Term Voltage","50","mV"
"Advanced Charge Algorithm","Cell Balancing Config","Bal Time/mAh Cell 1","301","s/mAh"
"Advanced Charge Algorithm","Cell Balancing Config","Bal Time/mAh Cell 2","307","s/mAh"
"Advanced Charge Algorithm","Cell Balancing Config","Min Start Balance Delta","3","mV"
"Advanced Charge Algorithm","Cell Balancing Config","Relax Balance Interval","18000","s"
"Advanced Charge Algorithm","Cell Balancing Config","Min Rsoc for Balancing","80","%"
"Gas Gauging","Current Thresholds","Dsg Current Threshold","20","mA"
"Gas Gauging","Current Thresholds","Chg Current Threshold","25","mA"
"Gas Gauging","Current Thresholds","Quit Current","1","mA"
"Gas Gauging","Current Thresholds","Dsg Relax Time","1","s"
"Gas Gauging","Current Thresholds","Chg Relax Time","60","s"
"Gas Gauging","Standby","StandbyCurrent","-10","mA"
"Gas Gauging","Max Load","Max Load Current","-500","mA"
"Gas Gauging","Max Load","Max Load Rsoc","50","%"
"Gas Gauging","Design","Design Capacity mAh","23200","mAh"
"Gas Gauging","Design","Design Capacity cWh","17168","cWh"
"Gas Gauging","Design","Design Voltage","8400","mV"
"Gas Gauging","Cycle","Cycle Count Percentage","90","%"
"Gas Gauging","FD","Set Voltage Threshold","3000","mV"
"Gas Gauging","FD","Clear Voltage Threshold","3100","mV"
"Gas Gauging","FD","Set % RSOC Threshold","0","%"
"Gas Gauging","FD","Clear % RSOC Threshold","5","%"
"Gas Gauging","FC","Set Voltage Threshold","4200","mV"
"Gas Gauging","FC","Clear Voltage Threshold","4100","mV"
"Gas Gauging","FC","Set % RSOC Threshold","100","%"
"Gas Gauging","FC","Clear % RSOC Threshold","95","%"
"Gas Gauging","TD","Set Voltage Threshold","3200","mV"
"Gas Gauging","TD","Clear Voltage Threshold","3300","mV"
"Gas Gauging","TD","Set % RSOC Threshold","6","%"
"Gas Gauging","TD","Clear % RSOC Threshold","8","%"
"Gas Gauging","TC","Set Voltage Threshold","4200","mV"
"Gas Gauging","TC","Clear Voltage Threshold","4100","mV"
"Gas Gauging","TC","Set % RSOC Threshold","100","%"
"Gas Gauging","TC","Clear % RSOC Threshold","95","%"
"Gas Gauging","State","Cycle Count","4","-"
"Gas Gauging","State","Qmax Cell 1","21820","mAh"
"Gas Gauging","State","Qmax Cell 2","21844","mAh"
"Gas Gauging","State","Qmax Pack","21820","mAh"
"Gas Gauging","State","Qmax Cycle Count","4","-"
"Gas Gauging","State","Update Status","0e","-"
"Gas Gauging","State","Cell 1 Chg Voltage at EoC","4308","mV"
"Gas Gauging","State","Cell 2 Chg Voltage at EoC","4304","mV"
"Gas Gauging","State","Current at EoC","243","mA"
"Gas Gauging","State","Avg I Last Run","-3075","mA"
"Gas Gauging","State","Avg P Last Run","-2237","cW"
"Gas Gauging","State","Delta Voltage","250","mV"
"Gas Gauging","State","Temp k","3.88","°C/256mW"
"Gas Gauging","State","Temp a","598","s"
"Gas Gauging","State","Max Avg I Last Run","-3091","mA"
"Gas Gauging","State","Max Avg P Last Run","-2489","cW"
"Gas Gauging","IT Cfg","Load Select","7","-"
"Gas Gauging","IT Cfg","Load Mode","0","-"
"Gas Gauging","IT Cfg","User Rate-mA","0","mA"
"Gas Gauging","IT Cfg","User Rate-cW","0","cW"
"Gas Gauging","IT Cfg","Reserve Cap-mAh","0","mAh"
"Gas Gauging","IT Cfg","Reserve Cap-cWh","0","cWh"
"Gas Gauging","IT Cfg","Design Resistance","10","mOhm"
"Gas Gauging","IT Cfg","Pack Resistance","30","mOhm"
"Gas Gauging","IT Cfg","System Resistance","0","mOhm"
"Gas Gauging","IT Cfg","Ra Filter","80.0","%"
"Gas Gauging","IT Cfg","Ra Max Delta","15","%"
"Gas Gauging","IT Cfg","Resistance Parameter Filter","65142","-"
"Gas Gauging","IT Cfg","Near EDV Ra Param Filter","59220","-"
"Gas Gauging","IT Cfg","Qmax Delta","5","%"
"Gas Gauging","IT Cfg","Qmax Upper Bound","130","%"
"Gas Gauging","IT Cfg","Term Voltage","6000","mV"
"Gas Gauging","IT Cfg","Term V Hold Time","1","s"
"Gas Gauging","IT Cfg","Term Voltage Delta","300","mV"
"Gas Gauging","IT Cfg","Term Min Cell V","2800","mV"
"Gas Gauging","IT Cfg","Fast Scale Start SOC","10","%"
"Gas Gauging","IT Cfg","Min Delta Voltage","250","mV"
"Gas Gauging","Smoothing","Smooth Relax Time","1000","s"
"Gas Gauging","Condition Flag","Max Error Limit","100","%"
"Power","Power","Valid Update Voltage","2800","mV"
"Power","Shutdown","Shutdown Voltage","2300","mV"
"Power","Shutdown","Shutdown Time","10","s"
"Power","Shutdown","Charger Present Threshold","3000","mV"
"Power","Sleep","Sleep Current","10","mA"
"Power","Sleep","Bus Timeout","5","s"
"Power","Sleep","Voltage Time","5","s"
"Power","Sleep","Current Time","20","s"
"Power","Sleep","Wake Comparator","00","hex"
"Power","Ship","FET Off Time","10","s"
"Power","Ship","Delay","20","s"
"Power","Ship","Auto Ship Time","1440","min"
"PF Status","Device Status Data","Safety Alert A","00","hex"
"PF Status","Device Status Data","Safety Status A","00","hex"
"PF Status","Device Status Data","Safety Alert B","00","hex"
"PF Status","Device Status Data","Safety Status B","00","hex"
"PF Status","Device Status Data","Safety Alert C","00","hex"
"PF Status","Device Status Data","Safety Status C","00","hex"
"PF Status","Device Status Data","Safety Alert D","00","hex"
"PF Status","Device Status Data","Safety Status D","00","hex"
"PF Status","Device Status Data","PF Alert A","00","hex"
"PF Status","Device Status Data","PF Status A","00","hex"
"PF Status","Device Status Data","PF Status D","00","hex"
"PF Status","Device Status Data","Operation Status A","0000","hex"
"PF Status","Device Status Data","Operation Status B","0000","hex"
"PF Status","Device Status Data","Temp Range","00","hex"
"PF Status","Device Status Data","Charging Status A","00","hex"
"PF Status","Device Status Data","Charging Status B","00","hex"
"PF Status","Device Status Data","Gauging Status","00","hex"
"PF Status","Device Status Data","IT Status","0000","hex"
"PF Status","Device Voltage Data","Cell 1 Voltage","0","mV"
"PF Status","Device Voltage Data","Cell 2 Voltage","0","mV"
"PF Status","Device Voltage Data","Battery Direct Voltage","0","mV"
"PF Status","Device Voltage Data","Pack Voltage","0","mV"
"PF Status","Device Current Data","Current","0","mA"
"PF Status","Device Temperature Data","Internal Temperature","-273.2","°C"
"PF Status","Device Temperature Data","External 1 Temperature","-273.2","°C"
"PF Status","Device Temperature Data","External 2 Temperature","-273.2","°C"
"PF Status","Device Gauging Data","Cell 1 Dod0","0","-"
"PF Status","Device Gauging Data","Cell 2 Dod0","0","-"
"PF Status","Device Gauging Data","Passed Charge","0","mAh"
"PF Status","AFE Regs","AFE Interrupt Status","00","hex"
"PF Status","AFE Regs","AFE FET Status","00","hex"
"PF Status","AFE Regs","AFE RXIN","00","hex"
"PF Status","AFE Regs","AFE Latch Status","00","hex"
"PF Status","AFE Regs","AFE Interrupt Enable","00","hex"
"PF Status","AFE Regs","AFE FET Control","00","hex"
"PF Status","AFE Regs","AFE RXIEN","00","hex"
"PF Status","AFE Regs","AFE RLOUT","00","hex"
"PF Status","AFE Regs","AFE RHOUT","00","hex"
"PF Status","AFE Regs","AFE RHINT","00","hex"
"PF Status","AFE Regs","AFE Cell Balance","00","hex"
"PF Status","AFE Regs","AFE AD/CC Control","00","hex"
"PF Status","AFE Regs","AFE ADC Mux","00","hex"
"PF Status","AFE Regs","AFE LED Output","00","hex"
"PF Status","AFE Regs","AFE State Control","00","hex"
"PF Status","AFE Regs","AFE LED/Wake Control","00","hex"
"PF Status","AFE Regs","AFE Protection Control","00","hex"
"PF Status","AFE Regs","AFE OCD","00","hex"
"PF Status","AFE Regs","AFE SCC","00","hex"
"PF Status","AFE Regs","AFE SCD1","00","hex"
"PF Status","AFE Regs","AFE SCD2","00","hex"
"System Data","Manufacturer Data","Manufacturer Info Block A01","61","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A02","62","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A03","63","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A04","64","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A05","65","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A06","66","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A07","67","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A08","68","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A09","69","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A10","6a","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A11","6b","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A12","6c","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A13","6d","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A14","6e","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A15","6f","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A16","70","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A17","71","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A18","72","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A19","73","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A20","74","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A21","75","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A22","76","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A23","77","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A24","7a","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A25","78","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A26","79","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A27","30","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A28","31","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A29","32","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A30","33","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A31","34","Hex"
"System Data","Manufacturer Data","Manufacturer Info Block A32","35","Hex"
"System Data","Integrity","Static DF Signature","0000","hex"
"System Data","Integrity","Static Chem DF Signature","5119","hex"
"System Data","Integrity","All DF Signature","0000","hex"
"I2C Configuration","Data","Manufacture Date","1980-1-1","date"
"I2C Configuration","Data","Serial Number","0001","hex"
"I2C Configuration","Data","Manufacturer Name","Texas Instruments","-"
"I2C Configuration","Data","Device Name","bq28z610","-"
"I2C Configuration","Data","Device Chemistry","LION","-"
"Lifetimes","Voltage","Cell 1 Max Voltage","0","mV"
"Lifetimes","Voltage","Cell 2 Max Voltage","0","mV"
"Lifetimes","Current","Max Charge Current","0","mA"
"Lifetimes","Current","Max Discharge Current","0","mA"
"Lifetimes","Temperature","Max Temp Cell","-128","°C"
"Lifetimes","Temperature","Min Temp Cell","127","°C"
"Ra Table","R_a0","Cell0 R_a flag","0055","-"
"Ra Table","R_a0","Cell0 R_a 0","9","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 1","9","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 2","9","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 3","11","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 4","11","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 5","9","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 6","10","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 7","8","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 8","9","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 9","11","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 10","15","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 11","22","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 12","41","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 13","74","2^-10ohm"
"Ra Table","R_a0","Cell0 R_a 14","1480","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a flag","0055","-"
"Ra Table","R_a1","Cell1 R_a 0","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 1","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 2","5","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 3","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 4","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 5","5","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 6","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 7","5","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 8","5","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 9","6","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 10","9","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 11","13","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 12","24","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 13","43","2^-10ohm"
"Ra Table","R_a1","Cell1 R_a 14","861","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a flag","0000","-"
"Ra Table","R_a0x","xCell0 R_a 0","9","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 1","9","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 2","11","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 3","14","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 4","13","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 5","11","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 6","12","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 7","10","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 8","11","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 9","14","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 10","18","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 11","27","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 12","50","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 13","90","2^-10ohm"
"Ra Table","R_a0x","xCell0 R_a 14","1809","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a flag","0000","-"
"Ra Table","R_a1x","xCell1 R_a 0","6","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 1","6","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 2","7","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 3","9","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 4","8","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 5","7","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 6","8","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 7","7","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 8","7","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 9","9","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 10","12","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 11","18","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 12","33","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 13","60","2^-10ohm"
"Ra Table","R_a1x","xCell1 R_a 14","1206","2^-10ohm"
Bq28z610_v1.6_04_11_Full_23200.txtBq28z610_v1.6_30_10_Full_23200 (1).txt

Waiting for your reply

Thanks

Star

  • Hello Star,

    I will take a look at this more tomorrow.

    The gauge should change the FCC and RemCap as there is a charge and temperature/current changes this is normal. For problem 1, this seems like normal operation.

    For problem 2 the gauge should be seeing the current and adjust according, your dsg current threshold and quit current may affect how the gauge reads the current, or if the gauge is in sleep mode.

    Sincerely,

    Wyatt Keller

  • Hi Wyatt Keller

    Thanks for your reply.

    For example, the RM value is 22300mah while the True RemCap value is 22500mah. Now the discharge process has started. There is no change in the RM value, but the True RemCap value decreases. When the True RemCap value is below the RM value, the RM Value drops abruptly.

    Why are the RM value and the True RemCap value not the same? How to Solve this Problem? Any Solution...

    My Product average current is 12mA and  My Gauge setting: DSG current threshold value is 20mA and quit current value is 1 mA. Is this correct or not? Need to make any changes to the setting?

    Waiting for your reply.

    Thanks

    Star

  • Hello Star,

    I took a look at your logs, it looks like the OCVFR flag is set during the cycle, what chemistry ID are you using?

    The RemCap has a filtered option, if the SMOOTH function is enabled the jumps should be mitigated. The two values of RemCap should not be the same because they are calculated with different smoothing factors.

    If you want the gauge to be measuring the 12mA more often then it would be best to set it lower to 10mA.

    Sincerely,

    Wyatt Keller

  • Hi Wyatt Keller

    Thanks for your reply.

    I used 0238 Chemistry ID. I will set the DSG current threshold value below 10 mA.

    My Design Capacity is 23200mAh(2s8p). Single Cell: Panasonic NCR 18650f(2900 mah) Battery.

    For example, the RM value is 22300mah while the True RemCap value is 22500mah. Now the discharge process has started. There is no change in the RM value, but the True RemCap value decreases. This condition persists for a long time. When the True RemCap value is below the RM value, the RM Value drops abruptly.

    Why this problem occurs? 

    Thanks

    Star

  • Hello Star,

    Do you have LOCK0 active? This may hold the RemCap SBS register. Also make sure the IT is enabled.

    Can you share the GPCCHEM report? Unless the ID was chosen because exact cell ID match.

    It looks like from the learning cycle log you shared that the Trem RemCap went below 0 as well, was that the successful learning cycle log?

    Sincerely,

    Wyatt Keller

  • Hi Wyatt Keller

    Thanks for your reply.

    The Lock0 Is enabled.

    The file(GPC Report) is attached here.

    GPC_Report-report.zip

    Thanks

    Star

  • Hello Star,

    The GPCCHEM report looks like a good match.

    Can you share a log file of this behavior after the learning cycle? The real testing for gauging accuracy should be after the learning cycle.

    Sincerely,

    Wyatt Keller